Search found 125 matches
- Wed Nov 27, 2024 11:26 pm
- Forum: Nerian Support Forum
- Topic: IMU position relative to cameras
- Replies: 5
- Views: 140649
Re: IMU position relative to cameras
Hi Jan, this is the data sheet for the IMU inside Scarlet: https://www.bosch-sensortec.com/media/boschsensortec/downloads/datasheets/bst-bno055-ds000.pdf The output characteristics for the accelerometer (linear accelerations) and gyroscope (angular velocities) can be found on pages 14 to 16. For the...
- Fri Nov 15, 2024 2:50 pm
- Forum: Nerian Support Forum
- Topic: IMU position relative to cameras
- Replies: 5
- Views: 140649
Re: IMU position relative to cameras
Hi, The rotation axes should be aligned with the coordinate system of the 3D point cloud (that is z-axis is the depth axis). I measured the offset of the IMU relative to the center of the left image sensor is. This is: Along the baseline (X): 145.6mm Vertically (Y): 13.1mm above the image sensor cen...
- Thu Jun 27, 2024 8:08 am
- Forum: Nerian Support Forum
- Topic: How can i get color image?
- Replies: 2
- Views: 73501
Re: How can i get color image?
Hi, according to your screenshot, your Karmin3 camera is a Mono model, so you will not be able to receive a color image from it. Karmin3 is available with monochrome and color image sensors. For depth measurement accuracy, monochrome sensors are preferred due to the superior image quality (higher sh...
- Thu Jun 13, 2024 6:51 am
- Forum: Nerian Support Forum
- Topic: Issus in SceneScan Pro Help: NVcom and visiontransferLibrary Issues
- Replies: 3
- Views: 84694
Re: Issus in SceneScan Pro Help: NVcom and visiontransferLibrary Issues
Hi, according to your screenshot, Jumbo frames are enabled on the device. Can you please verify that Jumbo are also enabled on the host PC? Please see the current manual on page 13: https://en.nerian.alliedvision.com/nerian-content/downloads/manuals/scenescan/scenescan_manual_v1_18.pdf Also, accordi...
- Tue May 28, 2024 2:05 pm
- Forum: Nerian Support Forum
- Topic: Image Stitching
- Replies: 2
- Views: 72827
Re: Image Stitching
Hi Jan, do you mean to stitch the left and right camera image into a single image? As the cameras share mostly the same field-of-view, there wouldn't be very much image data gained. In the best case (an object placed at the minimum measurable depth), the increased field-of-view due to stitching woul...
- Mon Apr 08, 2024 9:45 am
- Forum: Nerian Support Forum
- Topic: Stuck at "Ask parameter server to set stereo mode ..."
- Replies: 3
- Views: 89376
Re: Stuck at "Ask parameter server to set stereo mode ..."
Hi Jan,
thank you for the update. I'm glad the issue is resolved.
Best regards,
Konstantin
thank you for the update. I'm glad the issue is resolved.
Best regards,
Konstantin
- Thu Apr 04, 2024 9:57 am
- Forum: Nerian Support Forum
- Topic: Stuck at "Ask parameter server to set stereo mode ..."
- Replies: 3
- Views: 89376
Re: Stuck at "Ask parameter server to set stereo mode ..."
Hi Jan, this is indeed a strange behavior. The multi-cast network communication that we use for device enumeration worked, but creating a connection seems to fail. First of all, you can delete lines 50 and 51 from the example and it should still work. What these two lines do is create a connection t...
- Tue Dec 05, 2023 11:57 am
- Forum: Nerian Support Forum
- Topic: System hangs when fetching images from SceneScanPro
- Replies: 3
- Views: 86628
Re: System hangs when fetching images from SceneScanPro
Hi Saurabh, Alright, let me know when you need further help. Also: when using multiple SceneScans please put considerations into how they are connected. Each SceneScan can produce up to 900 MBits/s traffic on the link. So connecting multiple SceneScans through a single 1 Gigabit Link would not work....
- Thu Nov 09, 2023 10:57 am
- Forum: Nerian Support Forum
- Topic: Connect Problem
- Replies: 5
- Views: 120960
Re: Connect Problem
Hi, 1. According to your screenshot, Jumbo frames are not enabled for the two network interfaces (MTU = 1500 bytes). Could you please follow the instructions from the Manual to enable Jumbo Frames? 2. Is it possible that your PC and SceneScan are in different subnets? In that case the broad-cast mes...
- Tue Nov 07, 2023 10:02 am
- Forum: Nerian Support Forum
- Topic: Re: Issues in getting started with SceneScan Pro
- Replies: 5
- Views: 122620
Re: Re: Issues in getting started with SceneScan Pro
Hi,
I think my colleague has already reached out to you. Could you please return the device so we can address the issues.
Best regards,
Konstantin
I think my colleague has already reached out to you. Could you please return the device so we can address the issues.
Best regards,
Konstantin