Page 1 of 1

IMU position relative to cameras

Posted: Wed Nov 13, 2024 9:09 am
by ogrinj
Hi there,

Our company owns Nerian Scarlet (25cm) and we want to use it for real time stereo vision + IMU SLAM, which it is advertised for. We were able to obtain both visual (left and right image) and IMU data using slightly modified ros1 node and record a bag, however we were unable to find transformation matrix (rotation and translation) between coordinate systems of (at least one) camera and IMU, which we need in order to use SLAM algorithm. Where can we find this information? I checked both Scarlet manual and forum unsuccessfully. Please help.

Kind regards,
Jan

Re: IMU position relative to cameras

Posted: Thu Nov 14, 2024 10:43 am
by ogrinj
If there is no such data available (IMU-Cam calibration is not performed before Scarled being sold) I'll just perform the calibration process myself, I was just hopping I could avoid it :D

Re: IMU position relative to cameras

Posted: Fri Nov 15, 2024 2:50 pm
by k.schauwecker
Hi,

The rotation axes should be aligned with the coordinate system of the 3D point cloud (that is z-axis is the depth axis). I measured the offset of the IMU relative to the center of the left image sensor is. This is:

Along the baseline (X): 145.6mm
Vertically (Y): 13.1mm above the image sensor center
Depth (Z): 23 mm behind the image sensor

Best regards,
Konstantin

Re: IMU position relative to cameras

Posted: Mon Nov 18, 2024 2:04 pm
by ogrinj
Hi Konstantin,

thank you very much.

Kind regards,
Jan

Re: IMU position relative to cameras

Posted: Tue Nov 26, 2024 1:07 pm
by ogrinj
Hi Konstantin,

A follow-up question. We were able to use information from previous message to run stereo visual SLAM with our Nerian Scarlet also using IMU but algorithm diverges for some reason. It converges when we use only stereo visual SLAM but as soon as we use IMU data, it always diverges and we've gotten the same results with other stereo visual SLAM algorithms. This is why we suspected there might be something wrong with IMU data. We therefore recorded a ROS bag when camera was still/not moving. And identified strange behavior (see appended image of IMU data):

1) angular velocity data is much more smooth (approx. 4-times) i.e. observe flat lines in linear acceleration data in all axes where value is assumed to be constant (all values are sampled at the same frequency but linear acceleration data behaves as if it doesn't get values )

2) changes in linear acceleration data always happens at the same moment for all 3 axes.

Any ideas why this is happening? Also, have you or anyone else tested stereo visual + IMU SLAM with Nerian Scarlet? If so, can you share repository?

Kind regards,
Jan

Re: IMU position relative to cameras

Posted: Wed Nov 27, 2024 11:26 pm
by k.schauwecker
Hi Jan,

this is the data sheet for the IMU inside Scarlet:
https://www.bosch-sensortec.com/media/boschsensortec/downloads/datasheets/bst-bno055-ds000.pdf

The output characteristics for the accelerometer (linear accelerations) and gyroscope (angular velocities) can be found on pages 14 to 16.

For the accelerometer, there is an expected 2% cross axes sensitivity. In the real-world I would expect a stronger coupling, as it is difficult to perfectly stimulate only one axis.

We have other customers who are using Scarlet or Ruby in SLAM applications (both use the same IMU), but unfortunately we have no insight into their software.

If you are using our ROS node, please be aware that it transforms the 3D pointcloud coordinate system from our coordinate system (z pointing forward) to the ROS coordinate system (z pointing upwards) if the parameter ros_coordinate_system is set to true. If you use this feature you need to make sure that the IMU data is transformed accordingly.

Best regards,
Konstantin